EN | FR
Home  : FAQ

Frequently asked questions

Search a question
Select a topic
 
 Question/Reply per page
Show /hide

What does a UPS do ?

The distribution of electrical power is often subject to short and long term interference. Using an instantaneous back-up power supply means you can protect your IT system against such interference which can come from the industrial and atmospheric environment, as well as from your own environment. The following table lists the most common sorts of power supply problems, and the consequences for badly protected users:

CAUSES CONSEQUENCES
Voltage reduction  
Due to high voltage consumption required when starting up heavy equipment (motors, escalators, compressors, etc). Keyboard lock, system breakdown leading to data distortion or loss, reduction in equipment performance and lifespan.
Excess voltage  
Lightning hitting power cables or the sudden shutdown of high-consumption equipment can cause temporary voltage increase. Breakdowns, electronic component wear-and-tear, destruction of hard disks.
Cut-offs and micro cut-offs  
There can be many factors: lightning, live-line working, or heavy demand on the electrical network, etc. Data-loss, badly shut-off applications, equipment damage and problems when re-activating applications.
Stray  
There can be many factors: atmospheric conditions, load permutations, generators, radio-emitters, household and industrial equipment. Program and database errors.
Shock waves  
These are generally caused by lightning or when the mains supply is re-established after having been absent during a storm or following a motoring accident. Badly damaged components and equipment, data-loss..

Show /hide

What are criteria for choosing a UPS ?

Show /hide

What are the differences between On-line, Off-line or Line-interactive technologies ?

Show /hide

Is it necessary to protect a printer with a UPS ?

Show /hide

Is it necessary to protect a fax machine with a UPS ?

Show /hide

Are there any norms or standards concerning the choice of a UPS ?

Show /hide

Do I need a communication software ?

Show /hide

Do I need a UPS in addition to a gen-set ?

Show /hide

Is there a maximum ambient temperature for the correct operation of a UPS ?

Show /hide

What is the VSS+ DC?